Other Parts Discussed in Thread: AWR1443
Hello,
we have again an issue with the I2C clock frequency. This time on the IWR6843.
We use SDK 3.3.03 with target frequency of 400 kHz.
The IWR6843 outputs only 380kHz, while AWR1443 with the same code and same SDK driver code outputs exactly 400kHz.
By the way, this is exactly the inverted issue we once had with AWR1443 (see issue "AWR1443: I2C master frequency inaccurate"). It had been fixed by modifying a "magical number" in the SDK I2C driver code.
Following the reference manual swru522d, which was updated in the meantime, the formulas are correct. But the device does not behave according to the spec.
Please provide a reliable explanation.
Regards, Benjamin