Hi:
I'm evaluating the PGA460 for a battery operated product, and wanted to approximate the power consumption the device would require if it was, for example, reading for an object from 5cm-40cm away, with ten samples a second.
What I did was: Assume a burst of 170us, a listening period of 2.5ms (time sound takes to go 40cm and back at room temperature), and sleep afterwards.
I got it would be in burst mode for 0.17ms * 10 SPS = 1.7ms, @ 400mA
Listening for 2.5ms * 10SPS = 25ms @ 12mA
Sleep mode for the rest of the time (consuming 500uA).
Is this a fair assumption? Or am I missing something?
Thanks!
-Eduardo