This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91050: Output stays 0

Part Number: LMP91050


Hi team,

My customer now uses LMP91050, but after they power on the device and write 0x0060 to device, the LMP91050 still stays 0 when signal voltage is 1mV. Please see the attached schematic and SPI waveform. Is there anything need to be changed? Thank you.

  

LMP91050sch.pdf

  • Dear Taoran -

    in the schematic that was shared - it looks ok, however there is are components around the sensor which i cannot find that we recommend to place. 

    (their R1, R2, R3, C1)

    then - it seems from the o'scope image that they are intending to write into register 0 and they are changing the gain from default to 32. 

    Based on the thermopile characteristics (they need to check this with vendor), select the common-mode voltage and gain to be programmed into the LMP91050. CMOUT should be selected to center the expected dynamic range of the thermopile within the full scale range of the ADC to the best extent possible.

    The gain should be selected to maximize the signal range at the ADC input, but should allow some headroom below full scale to prevent clipping. The gain should also compensate, if possible, for any loss due to the filters in the signal path.

    I would highly recommend they get the evaluation kit and refer to it while developing

    LMP91050 eval board

    user guide

    code example

    board to use with eval board for to PC/GUI

  • Hi Josh,

    Thank you for your kindly help. 

    R1,R2,R3 and C1 is placed according to sensor datasheet. And now even if they input 0V I suppose there will be at least common mode voltage output.

    Can we confirm that the schematic(apart from sensor circuit) and SPI timing is correct ?

    Thank you

    Gary

  • Gary - 

    i cannot tell what the SPI clock timing is easily from the image sent over. The max SPI clock speed for this device is rated at 10MHz. The SPI timing characteristics are in the datasheet starting on page 6. http://www.ti.com/lit/ds/symlink/lmp91050.pdf