Other Parts Discussed in Thread: AWR1243,
Dear TI Team ,
We are a R&D team trying to build a Traffic density/ participant classification POC using AWR1243 BOOST evaluation board ( classes are Pedestrian, 2-Wheeler, 3-Wheeler , Passenger car , Truck , etc, ) , the kit was mounted on traffic pole of height approximately 5 to 15m with tiled angle towards ground looking to monitor traffic flow . We are unable to get the range and subsequently unable to classify targets beyond 4mts ,
Q1. Can we use AWR1243 Boost evel kit for traffic participant classification as the mounting is different than ADAS/AD applications ?
Q2. How do we get the max range for covering single and multiple lanes ?.
Thanks
Srinivas
+91-9448735252