This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT9221: Reset timing and signals

Part Number: OPT9221


The documentation outlines the power up sequence. But there is no description or timing diagram showing the reset process. Ideally, we need a similar diagram for the reset process. Hence, the following questions:

1) To use the RESETZ to apply soft reset, what is signal transition level? So, we nned the inactive level (high or low) and active/asserted level

2) Is there a minimum pulse duration for applying RESETZ? If so, how much

3) When RESETZ is asserted/enabled, what other (INT_OUT, TIC_CONF_DONE, etc.) change state?

Mo