Other Parts Discussed in Thread: AWR1843, UNIFLASH, MMWAVE-SDK
Hi all,
AWR1843 SBL over CAN
After I flashed the image "xwr18xx_sbl_demo.bin" using uniflash:
- Back SOP2 to operation
- Connect the serial com sniffer to User port as specified
- Reset the system by pressing SW2
- I get in the terminal screen:
**********************************************
Debug: Secondary Bootloader Application Start
**********************************************
Press any key to stop auto boot and Update Meta Image...
Loading existing Meta Image from Flash in 20 19 18 17 16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1
Debug: Device info: Manufacturer: 0, Device type = 0, Capacity = 0
Debug: Loading application metaImage from Flash address: c0040000
Error: Meta header absent!!!
Error: Could not download the metaimage to RAM. Trying to boot the backup factory default image.
Debug: Loading backup factory default image from Flash address: c0180000
Error: Meta header absent!!!
Error: Could not download the backup factory default image metaimage to RAM. Resetting the board to retry
************************************************
- According to the reference document I should get:
Debug: Device info: Manufacturer: 1, Device type = 40, Capacity = 16
Cannot go further...
Thanks,
Claudio