This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Testing moving OBJ question

  • Hi,

    1. Are you using the demo oob or did you make any changes to it?

    In our testing we are able to see at boresight a moving car at a range of ~80m with the configuration provided.

    If the object you are observing is smaller than a car than it is possible that it is observed at shorter range.

    2. This question is difficult to answer without more information and even raw data. Is this effect always observable? It would be better to test in an open environment first where there are no other cars moving.

    thank you

    Cesar