There are two pins on J6 - SYNC_In and SYNC_OUT. I have read on other threads these either can start the frame, or indicate that the frame is starting. For SYNC_IN you need to mount R165 zero ohm resistor and feed the pulse on the J6 connector pin #9. Is there an equivalent zero ohm resistor for SYNC_OUT.
Can you confirm that out of the box operation with just the AWR1642BOOST board while using the mmWave_Demo_Visualizer interface I can obtain a 3.3v frame trigger output, or provide a frame trigger externally.
Thanks