Hi all
We develop a Radar system for anti-collision of Crane.
We only want to detect and get the distance value of the crane (except other things).
Radar and Crane can be moving.
Which should I select ic between IWR and AWR series?
The Radar(mmWave IC) which can be used at an automobile has the wide-angle.
So it can be detected many things.
We only want to detect things which are selected by us.
It is similar to the cruise control system.
Is it possible to select a thing which we want to detect as the software?
We want to apply the mmWave IC the first time.
Is it possible to develop our application by mmWave IC of TI?