Hi,
I was wondering what the communication bus is after the radar signal processing pipeline is complete and we want to send out the data for further processing?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I was wondering what the communication bus is after the radar signal processing pipeline is complete and we want to send out the data for further processing?
Thanks!
Hello,
IWR6843 device is a Single Chip sensor with Integrated post processing capabilities. As such high level algorithms can be run on the deice.
Device Various peripherals available to get the processed data out of the device like SPI, Uart, I2c, CANFD,
FOr algorithm development highs speed Sensor Raw Data can be made available on LVDS port . YOu would need DCA1000 board for this.
Please let us know if that helps.
Vaibhav
Hi Vaibhav,
Thanks for the answer.
Just to clarify: can we send processed data through LVDS?
Thanks!
Dear anon:
To send processed data through LVDS you will need a DCA1000 board. Once you have a DCA1000 board you will need to follow the SDK user's guide which will elaborate using LVDS and the DCA1000 board.
Best regards,
Connor Desmond
Thanks for getting back to me Connor.
One more question:
Can we use LVDS to take data out of L3 memory? I am wondering what kinds of processing we can do before we send data through LVDS.
If we can take data out of L3 memory then we can send FFT data but if we can't then we will have to send classification data.
Thanks!
Dear anon1234566788:
I would suggest taking your questions and make a separate thread. This will get your questions answered more directly.
Best regards,
Connor Desmond