When CSI 2 is configured as two outputs, the data is only RX0, RX1. Does this mean that there are only two receiving antennas, and the other two receiving antennas are invalid?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When CSI 2 is configured as two outputs, the data is only RX0, RX1. Does this mean that there are only two receiving antennas, and the other two receiving antennas are invalid?