Other Parts Discussed in Thread: MMWCAS-DSP-EVM,
Hi, we are developping our own cascade RF board with 4 AWR1243P. We have run everything good with MMWCAS-RF-EVM and MMWCAS-DSP-EVM.
Then We try to run the master AWR1243P on our own RF board with MMWCAS-DSP-EVM. We modify the Cascade_Configuration_TestSource.lua to set only the master chip and the script run successfully. Then we start the Cascade_Capture.lua which is nothing modified. After starting the Framing_Control of the master chip, it reports: "[DeviceId-0] MSS ESM Fault error status Async event received(0x400000, 0x0)".
The test is using mmWaveStudio 2.1.0.0. The firmware is xwr12xx_metaImage.bin in mmwave_dfp_01_02_05_01 and is downloaded successfully by Cascade_Configuration_TestSource.lua. The AWR1243P status is XWR1243/ASIL-B/SOP:4/ES:3.
What is the problem? We only weld 1 chip for testing. Will it cause the problem?