Other Parts Discussed in Thread: AWR2243, , AWR1642, AWR1243
Hi everyone
We are looking for Radar Front-End solution for Anti-Collision.
1. Install
We will install the Radar between two moving Crane.
The Radar measures the distance of two cranes.
2. The angle.
we need narrow-angle of Radar.
Because there is much structure around the Cranes.
We only want to detect the Crane.
3. measurement
The most important is the distance between the two cranes.
One of them may stop, another one may move.
(Both can be a move or stop)
Any situation, the radar must measure the distance.
If another structure is detecting, we must ignore the distance of the structures or not detect it.
I'm thinking the ic whether AWR1843 or AWR2243.
we want to buy AWR1843(or AWR2243), how long take the delivery time?
Please recommend.
We pray for all of the worlds fighting to overcome the Corona-virus.
Take care your-self. From S.Korea