Other Parts Discussed in Thread: IWR6843, IWR1843BOOST
Hi,
We are encountering two kinds of issue with the IW6843-ISKODS 3D People Counting Demo:
1. The demo cannot run for more than 2 hours. After a while, it will crash and be resolved when we power down.
2. The demo cannot start even after sending the CFG commands successfully. The sensorStart command seems to break the USB connection and even powering down the device multiple times and reconnecting the USB don't solve the problem and we cannot start it for a while. When we are able to start again, we cannot figure out what made it work.
Do you have any idea what may have cause these 2 issues? We are encountering the same issues with IWR1846 Traffic Monitoring Demo. Both are ES2.0 devices and using the latest toolbox.
Thanks