For a project my team is designing, I need to know the maximum possible current draw for the breakaway board once separated. We are planning a power supply system and need the current to plan for power usage. I was unable to find the value listed.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For a project my team is designing, I need to know the maximum possible current draw for the breakaway board once separated. We are planning a power supply system and need the current to plan for power usage. I was unable to find the value listed.
Hello EightBitBoot,
Power consumption is function of chirp profile, Duty-cycle and use-case dependent. But high-level you should be able to operate with USB based power supply, i.e. 5V 500mA for most of the applications. For higher duty-cycled application power could go upto 600mA.
Thanks and regards,
CHETHAN KUMAR Y.B.