Other Parts Discussed in Thread: PGA460
hello,
I have this transducer www.chinalevelsensor.com/.../ and i want to know if i can connect it to the daughtercard. It needs at least 300V peak to peak.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello,
I have this transducer www.chinalevelsensor.com/.../ and i want to know if i can connect it to the daughtercard. It needs at least 300V peak to peak.
Hi Alex,
Yes, the TD40200D transducer is compatible with the PGA460. The transformer included with the BOOSTXL-PGA460 has a 1:1:10 turns ratio. This means when you supply the maximum allowable voltage of 15V at the center-tap of the transformer, you will generate +/-150V or 300Vpp.
Hi Alex,
Most transducers have an equivalent resistance of 1kOhm or larger, so the current will be in the mA range.
You can use an impedance analyzer to better approximate the equivalent circuit of your transducer if this information is not provided in the transducer datasheet. The "PGA460 Ultrasonic Module Hardware and Software Optimization" ( http://www.ti.com/lit/an/slaa732/slaa732.pdf ) app report describes using an impedance analyzer for this purpose.