Tool/software: Code Composer Studio
Dear TI
Which one is the default chirp setting of HAVC Lab ( Toolbox 4.2.1) ?
how to setting and modify these parameters ?
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Toyota,
By default, it is TDM-MIMO. BPM-MIMO is enabled in the hardware/BSS firmware, but has not been built into the software for the HVAC demo.
Regards,
Justin
Dear TI
Thank , one question is TDM-MIMO how to change the TX direction ? Our testing txPhaseShifter can be setting normal , but TDM-MIMO the TX channels not simultaneously output how to achieved this function ? TDM is time division not simultaneously.
BR
Hi Toyota-1,
This is controlled by the chirpCfg line in the configuration file. Please see the SDK user guide documentation on the configuration cli commands.
ProfileCfg controls the phase shift, there is a setting for each Tx.
ChirpCfg controls when a Tx is used. This is a multiplexed argument: chirpCfg 1 1 0 0 0 0 0 4 indicates the device will use Tx 3 when running this chirp, chirpCfg 1 1 0 0 0 0 0 5 indicates the device will use Tx 1 and Tx 3.
Regards,
Justin