Other Parts Discussed in Thread: MMWAVEICBOOST, , AWR1843BOOST, UNIFLASH
Hi to all,
I'm trying to run correctly the Unit Test of mmwavelink but I have problem even if I use the original bynaries.
Some information in order to describe my environment:
- I'm using the mmwave_sdk_03_03_00_03 version
- I'm using a IWR6843ISK-ODS installed on a MMWAVEICBOOST
- I have correctly loaded the xwr68xx_ccsdebug.bin that i have found in the sdk
- I have loaded the two binaries xwr68xx_link_dss.xe674 and xwr68xx_link_mss.xer4f
Then, I launch the test on DSS and the test seems blocked after a sensor Start. The console output shows:
[C674X_0] Debug: ADCBUF Instance @0081a180 has been reopened successfully
******************************************
Debug: Launching the mmwaveLink
******************************************
Debug: Launching BIOS
Debug: Launched the mmwaveLink Initialization Task
Debug: CRC Channel @008012f8 has been opened successfully
Debug: Launched the mmwaveLink Management Task
Debug: BSS Mailbox Handle @00801be8
Debug: Disabling the device
Debug: BSS Mailbox Handle @00801be8
Debug: Power on request successfully passed to the BSS
Feature: mmWave Link Initialization: Passed
Debug: BootupStatus = 8011f4
Debug: Finished get radarSS bootup status to BSS
Feature: Get radarSS bootup status: Passed
RF H/W Version : 02.00
RF F/W Version : 06.02.00.06.19.08.22
RF F/W Patch Version : 00.00.00.00.00.00.00
mmWaveLink Version: 01.02.05.16
Feature: Get mmWave Link Version: Passed
Debug: Finished rlRfSetDeviceCfg
Feature: Set Async event config: Passed
Debug: Set HSI clock successfully
Feature: Set HSI clock: Passed
Debug: Finished rlDeviceConfigureAckTimeout
Feature: Set ACK timeout to min value: Passed
Debug: Finished rlDeviceConfigureAckTimeout
Feature: Set ACK timeout to max value: Passed
Debug: Finished rlDeviceConfigureAckTimeout
Feature: Set ACK timeout: Passed
Feature: mmWave Link Negative Test: Passed
Debug: Die ID Status
Lot no : 9323977, Wafer no: 2031649
Die cordinates in wafer. X : 41 , Y : 0
Feature: Get Device Die ID Status: Passed
Debug: Finished set channel configurations to BSS
Feature: Set mmWave Link Channel Config: Passed
Debug: Finished setAdcOutConfig to BSS
Feature: Set mmWave Link ADC Out Config: Passed
Feature: mmWave Link Enable/Disable Calibration: Passed
Debug: Init time calibration status [0x8000001e]
Debug: RF start successfully
Feature: mmWave Link RF Calibration: Passed
Debug: Finished rlRfCalibDataStore
Feature: mmWave Link Calibration Data Store config: Passed
Feature: mmWave Link Enable/Disable Calibration: Passed
Debug: Init time calibration status [0x80000012]
Debug: Finished rlRfCalibDataRestore
Feature: mmWave Link Calibration Data Restore config: Passed
Debug: Init time calibration status [0x8000001e]
Debug: RF start successfully
Feature: mmWave Link RF Calibration: Passed
Debug: Finished rlSetGpAdcConfig
Feature: mmWave Link Set GPAdc: Passed
Debug: Finished rlRfSetLdoBypassConfig
Feature: mmWave Link Set LDO bypass: Passed
Feature: mmWave Link Calib/Monitoring config: Passed
Debug: Finished rlSetProfileConfig
Feature: Set mmWave Link Profile config: Passed
Debug: Finished rlRxGainTempLutGet
Feature: Get mmWave Link RX Gain Temperature LUT config: Passed
Debug: Finished rlTxGainTempLutGet
Feature: Get mmWave Link TX Gain Temperature LUT config: Passed
Debug: Finished rlRxGainTempLutSet
Feature: Set mmWave Link RX Gain Temperature LUT config: Passed
Debug: Finished rlTxGainTempLutSet
Feature: Set mmWave Link TX Gain Temperature LUT config: Passed
Debug: rlGetProfileConfig parameters matched with configured parameters
Feature: Get mmWave Link Profile config: Passed
Debug: Finished rlSetChirpConfig
Feature: Set mmWave Link Chirp config: Passed
Debug: Finished rlSetMultiChirpCfg
Feature: Set mmWave Link Multi Chirp config: Passed
Debug: Finished rlRfInterRxGainPhaseConfig
Feature: Set mmWave Link Inter RX Gain/Phase config: Passed
Debug : Temerature readings
RX0 : 43 degree C, RX1 : 42 degree C, RX2 : 40 degree C, RX3 : 42 degree C
TX0 : 44 degree C, TX1 : 43 degree C, TX2 : 46 degree C
PM : 46 degree C, DIG0: 49 degree C
Feature: Set mmWave Link Get Temperature Report: Passed
Debug: Finished rlSetTestSourceConfig
Debug: Finished rlTestSourceEnable
Feature: Set mmWave Link Test Source config: Passed
Debug: Finished rlSetFrameConfig
Feature: Set mmWave Link Frame config: Passed
Debug: rlGetFrameConfig parameters matched wilh configured parameters
Feature: Get mmWave Link Frame config: Passed
Debug: Finished rlRfSetPALoopbackConfig
Feature: Enable mmWave Link PA Loop Back config: Passed
Feature: Sensor Start: Passed
Is there something wrong in my way of launch the unit test?
Thanks,
Stefano