This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/PGA400-Q1: Not able to download GUI for PGA400-Q1 IC

Part Number: PGA400-Q1
Other Parts Discussed in Thread: PGA302, PGA300, PGA900, PGA305

Tool/software: WEBENCH® Design Tools

Hi,

I'm not able to download GUI of PGA400-Q1. From where i can download its GUI?

Thanks & Regards,

Amruta

  • Hello Amruta,

    Please go to the PGA400 page here: https://www.ti.com/product/PGA400-Q1

    Under "More Information" click to request the datasheet. Once you have been approved, the GUI is available in the mySecure Software page for the PGA400.

    Regards,

  • Hello Scott,

    Thanks for the reply.

    Also can i get sample program and programming guide for this IC which will accelerate our development process?

    Thanks & Regards,

    Amruta Tundurwar

  • Hi Amruta,

    Can you please give some more details about your application? Is this used for a pressure or current sensing application? Or some capacitive sensing? For pressure sensing in an automotive environment where Q1 qualification is needed I recommend looking into the PGA302 instead. It is currently only available in a commercial version, but an automotive qualified version is planned to be released this year. There will also be a PGA902 which uses the same analog front end and output stage but allows for programming of an internal M0 microcontroller with user-created firmware.

    The PGA305, PGA300, and PGA900 are all also good options for a pressure sensing application if automotive qualification is not needed.

    E2E support for firmware development for the PGA400 is limited at this point. There is some example code posted in this earlier thread on E2E: https://e2e.ti.com/support/data-converters/f/73/t/687713 but we cannot currently provide any additional development support outside of what is included in that package, and the PGA400 documentation already available on ti.com.

    Regards,

  • Hi Scott,

    It is for current sensing application. We are using SPI communication for it. But i'm not getting any SPI sequence writing sequence for programming PGA400Q1 IC. Also i'm not able to download the GUI for it.

    Please help me with it.

    Thanks & Regards,

    Amruta Tundurwar

  • Part Number: PGA400-Q1

    Tool/software: WEBENCH® Design Tools

    Hi,

    I want to download PGA400Q1 GUI. But i'm not getting link for it. Also i need the sequence for programming PGA400Q1 IC using SPI.

    Please help me with it.

    Thanks & Regards,

    Amruta Tundurwar

  • Hello Amruta,

    I've joined your new E2E thread to this original one. The full PGA400 datasheet includes the SPI programming procedure for the PGA400, and it is also available as part of the mysecure site where the PGA400EVM GUI is located. If you have submitted your request already, you will receive access to these items if your request is approved.

    Regards,

  • Hello Scott,

    Can you please help me to whom i can contact for the request approval?

    Thanks & Regards,

    Amruta Tundurwar

  • Hi Amruta, 

    Let me reach out to the people that support your account from TI. Would it be alright if we emailed you directly regarding this request?

    Thanks,