This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP100: Coefficient of thermal expansion (CTE)

Part Number: TMP100

Hi team,

Good day.

What is the CTE of TMP100NA/3K?


Regards,
Carlo

  • Hi Carlo,

    I am putting in a request with our packaging team for this information, and I will update this thread as soon as it is available.

    Typically these modeling requests take a week or two, but I will check around and see if I can get the information any faster. 

    Best Regards,
    Brandon Fisher

  • Hi Carlo,

    I apologize for the delay. The CTE for this part is as follows, please note that these are estimates:

    Temperature Range αX ppm/°C αY ppm/°C
    -40 to 120°C 11.0 13.4
    120 to 150°C 26.7 24.8

    Best Regards,
    Brandon Fisher