Hello,
I'd like to inquire about an incomprehensible phenomenon regarding the internal temperature sensor value of IWR1443.
Reading the internal temperature with SDK 2.0 at room temperature, the value of DIG0 is found to be 90℃, which is much higher than other sensors values. All other sensors have values of less than 55℃.
Is it normal that the temperature difference is greater than 35℃ at the same Die?
If this is normal, we cannot adopt this chip in our application because it easily exceeds the junction temperature 105 ℃ at an ambient temperature of 45 ℃ or more.
Best Regards,