Hi Experts,
How long does it take to complete boot time BIST on AWR1843?
Best regards,
Ken
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ken,
Many of BIST test are done during the boot up time. And bootup time can be read from BSS using rlGetRfBootupStatus API.
All the BIST test which it does will be within the bootup time received in above API response.
Regards,
Jitendra
Ken,
Boottime for BSS is ~10ms
Boot time for MSS is dependent on:
The boot time of ~100ms for a AWR1843 device boot .
BR,
Raghu