This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Data analysis

Part Number: IWR1642BOOST

Hi,

How to acquire data after 1D-FFT/2D-FFT/CFAR, are they stored in the buffer which can be used for analyze?

for example:C:mmwave_industrial_toolbox_4_2_1\labs\out_of_box_demo\16xx_mmwave_sdk

  • Former Member
    0 Former Member

    Hello,

    The data shown in the plots in the visualizer can be captured using the "Record Start" button in the visualizer. 

    To output all 1D FFT, 2D FFT, and detection matrix data would be difficult with the data rate limits of UART using the out of box demo. However the range profile and the range azimuth plots are the outputs of the 1D FFT and 2D FFT for the 0 doppler bin.

    Amanda