This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843: Can I use CLI to set CW mode for RF testing purpose?

Part Number: IWR1843


2020-04-27 13:55:17.391 sensorStop
2020-04-27 13:55:17.394 Ignored: Sensor is already stopped
2020-04-27 13:55:17.394
2020-04-27 13:55:17.394 Done sensorStop
2020-04-27 13:55:17.394
2020-04-27 13:55:17.394
2020-04-27 13:55:17.445 mmwDemo:/>flushCfg
2020-04-27 13:55:17.446 Done
2020-04-27 13:55:17.447
2020-04-27 13:55:17.448 Done flushCfg
2020-04-27 13:55:17.449
2020-04-27 13:55:17.449
2020-04-27 13:55:17.561 mmwDemo:/>dfeDataOutputMode 1
2020-04-27 13:55:17.563 Done
2020-04-27 13:55:17.564
2020-04-27 13:55:17.565 Done dfeDataOutputMode 1
2020-04-27 13:55:17.566
2020-04-27 13:55:17.566
2020-04-27 13:55:17.669 mmwDemo:/>channelCfg 15 1 0
2020-04-27 13:55:17.671 Done
2020-04-27 13:55:17.672
2020-04-27 13:55:17.673 Done channelCfg 15 1 0
2020-04-27 13:55:17.673
2020-04-27 13:55:17.674
2020-04-27 13:55:17.777 mmwDemo:/>adcCfg 2 1
2020-04-27 13:55:17.778 Done
2020-04-27 13:55:17.779
2020-04-27 13:55:17.781 Done adcCfg 2 1
2020-04-27 13:55:17.786
2020-04-27 13:55:17.787
2020-04-27 13:55:17.884 mmwDemo:/>adcbufCfg -1 0 1 1 1
2020-04-27 13:55:17.888 Done adcbufCfg -1 0 1 1 1
2020-04-27 13:55:17.890
2020-04-27 13:55:17.891
2020-04-27 13:55:17.994 mmwDemo:/>profileCfg 0 77 7 7 58 0 0  68 1 256 5500 0 0 30
2020-04-27 13:55:17.997 Done
2020-04-27 13:55:17.999
2020-04-27 13:55:18.000 Done profileCfg 0 77 7 7 58 0 0  68 1 256 5500 0 0 30
2020-04-27 13:55:18.001
2020-04-27 13:55:18.003
2020-04-27 13:55:18.050 mmwDemo:/>chirpCfg 0 0 0 0 0 0 0 1
2020-04-27 13:55:18.054 Done
2020-04-27 13:55:18.055
2020-04-27 13:55:18.056 Done chirpCfg 0 0 0 0 0 0 0 1
2020-04-27 13:55:18.058
2020-04-27 13:55:18.060
2020-04-27 13:55:18.162 mmwDemo:/>bpmCfg -1 0 0 1
2020-04-27 13:55:18.166 Done bpmCfg -1 0 0 1
2020-04-27 13:55:18.167
2020-04-27 13:55:18.170
2020-04-27 13:55:18.270 mmwDemo:/>frameCfg 0 1 32 0 800 1 0
2020-04-27 13:55:18.273 Done
2020-04-27 13:55:18.275
2020-04-27 13:55:18.277 Done frameCfg 0 1 32 0 800 1 0
2020-04-27 13:55:18.278
2020-04-27 13:55:18.280
2020-04-27 13:55:18.378 mmwDemo:/>lowPower 0 1
2020-04-27 13:55:18.382 Done
2020-04-27 13:55:18.384
2020-04-27 13:55:18.386 Done lowPower 0 1
2020-04-27 13:55:18.388
2020-04-27 13:55:18.389
2020-04-27 13:55:18.487 mmwDemo:/>guiMonitor -1 1 1 1 1 1 1
2020-04-27 13:55:18.490 Done guiMonitor -1 1 1 1 1 1 1
2020-04-27 13:55:18.492
2020-04-27 13:55:18.493
2020-04-27 13:55:18.596 mmwDemo:/>cfarCfg -1 0 2 8 4 3 0 15.0 0
2020-04-27 13:55:18.598 Done cfarCfg -1 0 2 8 4 3 0 15.0 0
2020-04-27 13:55:18.601
2020-04-27 13:55:18.601
2020-04-27 13:55:18.650 mmwDemo:/>cfarCfg -1 1 0 8 4 4 1 15.0 1
2020-04-27 13:55:18.655 Done cfarCfg -1 1 0 8 4 4 1 15.0 1
2020-04-27 13:55:18.656
2020-04-27 13:55:18.658
2020-04-27 13:55:18.758 mmwDemo:/>multiObjBeamForming -1 1 0.5
2020-04-27 13:55:18.762 Done multiObjBeamForming -1 1 0.5
2020-04-27 13:55:18.763
2020-04-27 13:55:18.765
2020-04-27 13:55:18.870 mmwDemo:/>calibDcRangeSig -1 0 -5 8 256
2020-04-27 13:55:18.872 Done calibDcRangeSig -1 0 -5 8 256
2020-04-27 13:55:18.872
2020-04-27 13:55:18.873
2020-04-27 13:55:18.985 mmwDemo:/>extendedMaxVelocity -1 0
2020-04-27 13:55:18.987 Done extendedMaxVelocity -1 0
2020-04-27 13:55:18.990
2020-04-27 13:55:18.991
2020-04-27 13:55:19.093 mmwDemo:/>clutterRemoval -1 0
2020-04-27 13:55:19.097 Done clutterRemoval -1 0
2020-04-27 13:55:19.097
2020-04-27 13:55:19.098
2020-04-27 13:55:19.150 mmwDemo:/>compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
2020-04-27 13:55:19.155 Done compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
2020-04-27 13:55:19.157
2020-04-27 13:55:19.159
2020-04-27 13:55:19.261 mmwDemo:/>measureRangeBiasAndRxChanPhase 0 1.5 0.2
2020-04-27 13:55:19.265 Done measureRangeBiasAndRxChanPhase 0 1.5 0.2
2020-04-27 13:55:19.266
2020-04-27 13:55:19.268
2020-04-27 13:55:19.371 mmwDemo:/>aoaFovCfg -1 -90 90 -90 90
2020-04-27 13:55:19.374 Done aoaFovCfg -1 -90 90 -90 90
2020-04-27 13:55:19.376
2020-04-27 13:55:19.377
2020-04-27 13:55:19.478 mmwDemo:/>cfarFovCfg -1 0 0.25 9.71
2020-04-27 13:55:19.481 Done cfarFovCfg -1 0 0.25 9.71
2020-04-27 13:55:19.483
2020-04-27 13:55:19.485
2020-04-27 13:55:19.586 mmwDemo:/>cfarFovCfg -1 1 -7.49 7.49
2020-04-27 13:55:19.590 Done cfarFovCfg -1 1 -7.49 7.49
2020-04-27 13:55:19.591
2020-04-27 13:55:19.592
2020-04-27 13:55:19.696 mmwDemo:/>CQRxSatMonitor 0 3 4 127 0
2020-04-27 13:55:19.698 Done CQRxSatMonitor 0 3 4 127 0
2020-04-27 13:55:19.701
2020-04-27 13:55:19.702
2020-04-27 13:55:19.752 mmwDemo:/>CQSigImgMonitor 0 63 8
2020-04-27 13:55:19.756 Done CQSigImgMonitor 0 63 8
2020-04-27 13:55:19.758
2020-04-27 13:55:19.759
2020-04-27 13:55:19.862 mmwDemo:/>analogMonitor 0 0
2020-04-27 13:55:19.865 Done analogMonitor 0 0
2020-04-27 13:55:19.866
2020-04-27 13:55:19.867
2020-04-27 13:55:19.973 mmwDemo:/>lvdsStreamCfg -1 0 0 0
2020-04-27 13:55:19.976 Done lvdsStreamCfg -1 0 0 0
2020-04-27 13:55:19.978
2020-04-27 13:55:19.979
2020-04-27 13:55:20.081 mmwDemo:/>dfeDataOutputMode 2
2020-04-27 13:55:20.084 Done
2020-04-27 13:55:20.086
2020-04-27 13:55:20.088 Done dfeDataOutputMode 2
2020-04-27 13:55:20.090
2020-04-27 13:55:20.091
2020-04-27 13:55:20.188 mmwDemo:/>contModeCfg 77 0 0 5500 0 0 30 1 512
2020-04-27 13:55:20.192 Done
2020-04-27 13:55:20.194
2020-04-27 13:55:20.197 Done contModeCfg 77 0 0 5500 0 0 30 1 512
2020-04-27 13:55:20.197
2020-04-27 13:55:20.198
2020-04-27 13:55:20.296 mmwDemo:/>sensorStart
2020-04-27 13:55:20.301 Debug: Init Calibration Status = 0x7fe

Hi,

 In order for the RF lab test and production line test purpose, I need to set the IWR1843 into CW mode. I know the mmWave Studio tool can do this, but I will need the easier CLI method due to lab or factory engineers might not be able to install the mmWave Studio.

 I tried to modify the cfg file to enable the continuous mode, and set the freq to 77GHz for 0 slope as below (detail commands are attached in "CLI for CW mode.txt" file). But the IWR1843 doesn't output anything.

 Is there any commands missing?

=====================================================================================

2020-04-27 13:55:20.081 mmwDemo:/>dfeDataOutputMode 2
2020-04-27 13:55:20.084 Done

2020-04-27 13:55:20.088 Done dfeDataOutputMode 2

2020-04-27 13:55:20.188 mmwDemo:/>contModeCfg 77 0 0 5500 0 0 30 1 512
2020-04-27 13:55:20.192 Done

2020-04-27 13:55:20.197 Done contModeCfg 77 0 0 5500 0 0 30 1 512

2020-04-27 13:55:20.296 mmwDemo:/>sensorStart
2020-04-27 13:55:20.301 Debug: Init Calibration Status = 0x7fe