This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Question related to RangeAzimuthHeatmap result of IWR6843 DEMO

Part Number: IWR6843

Hello,

I am running xwr68xx demo with iwr6843 which is included in mmwave SDK.

When I turn on RangeAizimuthHeatmap, sometimes I receive same Heatmaps for several frame(it lasts forever).

Since heatmap of each of frames are totally identical, it seems like sensor has stoped.

But sensor is keep working while just sending the same heatmap from frame to frame.

Is there any reason that might cause this kind of phenomenon.

Thank you in advance.

  • HI, 

    The UART may not have enough capacity to transfer data for rangeAzimuth heatmap generation, can you slow down the frame rate to 2 frames/second and try again.  And also disable other heavy data transfer like Range- Doppler heatmap.  

    Best,
    Zigang 

  • Hello Zigang,

    Thanks for the quick reply.

    I've only enabled Range Azimuth Heat map by setting guiMonitor config as below.

    guiMonitor -1 0 0 0 1 0 0

    Therefore the amount of data that I am capturing every frame is less than 8kb. 

    I though 8kb should not be a problem considering the UART capacity(UART baud rate for logging is 900kbs).

    Also, this phenomenon was frequently observed when the object is very close to the radar(around 10cm to 20cm)

    Does the distance from the radar might cause this problem?

    Thank you.

    Best regards,

    Yechan

  • Hi, Yechan:

    So do you have anything moving in front of the sensor?   Why you expect the heatmap to be changing?

    Best,

    Zigang

  • Hi, Zigang

    Yes the object in front the radar is moving object(periodically moving).

    So the heatmap should be changed.

    Even if there exist only static object on the field of view, the heat map values should be changed.

    But I got exactly same values from frame to frame.

    Best Regards,

    Yechan

  • HI, Yechan:

    The range azimuth heatmap is generated by calculate the zero Doppler.  If you have a target that are moving at a regular speed, the zero Doppler may not change.   Can you have a person walk and stop randomly in front of the sensor and check whether the range azimuth heatmap is changing?

    Why did you say that the purely static scene could still cause the change the heatmap?

    Best,

    Zigang 

  • HI, 

    I have not receive any reply from you for a week now.  I am closing this thread.

    Best,

    Zigang