Hi Team,
The datasheet tells the duty cycle peak-to-peak jitter is ±0.1%D, how to understand this spec?
For example, if the output duty cycle is 50% PWM when B is 0mT in theory, will the actual output duty be 49.9%(50%-0.1%)~50.1%(50%+0.1%) or 49.95%(50%-50%*0.1%)~50.05%(50%+50%*0.1%)?
Another question, will the output duty cycle change or keep the same when the temperature changes while B is constant? For example, if the output duty cycle is 50% PWM when B is 0mT at 25℃, will the output duty cycle still be 50% when the temperature is 50℃? If not, is there any tested data about the temperature drift for output duty cycle?
Thanks and Best Regards!
Hao