This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: I want to control AWR1843BOOST without SDK file

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: MMWAVE-SDK, AWR1843

Hello,

  I'm using 'Raspberry Pi 4 B' with OS 'Raspbian' and ARM architecture. This computer would be used for receiving data from AWR1843BOOST.

  During installing mmwave-sdk file, there was an error that 'execute binary file:Exec format error'. I tried many methods to install this, including change OS and converting from 32-bit to 64-bit. But I couldn't solve this issue. I guess this error was come from Architecture issue, I heard that many SDK file is compatible with intel architecture, not ARM.

  So, I'm thinking about connecting AWR1843BOOST and Raspberry pi via GPIO pins without SDK file. I'm not sure it's possible to do this. Could you give me the advice for this way?