I'm doing SPI test of IWR6843 EVM for many cases. About, 2 EVMs connection, I don't have to worry about the voltage difference. But I see IWR6843 EVM power input is 5V, while Arduino Uno is 6-12V. Please tell me whether IWR6843 EVM will be broken if I connect them directly. If yes, which device I should use as a level shifter between them?
- About Rapsberry Pi 3, I see the input voltage must be between 4.75 and 5.25V. So it should be ok to connect IWR6843 EVM directly to Pi 3.
Since I'm not professional in hardware & power, so I only assume above. I want TI engineers suggest me the way to connect IWR6843 EVM to Arduino/Pi 3, respectively. I'd appreciate if you could provide me with the name of level shifter (converter) and wiring diagram.