This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: People Counting with radar inside a plastic box IP65 (protection against water) - unable to detect objects

Part Number: AWR1642BOOST

Good afternoon,

I'd like to know what parameters should edit in the CFG file if we want to have the sensor inside a plastic box. 

But the detection becomes worse (doesn't detect people) went is inside a plastic box IP65 with a distance of 2.5cm between the antenna and the plastic box. Can anyone share how do you solve this issue? I think that the problem should be the same for other types of application or demo code with radar.

It's possible to buy a special box with protection for water (rain, water splashes, etc ...)?

At this moment I have the following CFG parameters:

dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg 0 1 1 1
profileCfg 0 77 30 7 62 0 0 60 1 128 2500 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 128 0 50 1 0
lowPower 0 1
guiMonitor 1 1 0 0
cfarCfg 6 4 4 4 4 16 16 4 4 50 62 0
doaCfg 600 1875 30 1
SceneryParam -6 6 0.05 14
GatingParam 4 3 2 0
StateParam 7 5 10 100 5
AllocationParam 100 0.01 18 1 2
VariationParam 0.289 0.289 1.0
PointCloudEn 1
trackingCfg 1 2 250 20 200 50 100
sensorStart

Thanks

Best Regards

André Dias