Hi
We are using the FDC1004 in a small size portable device with a very small battery. To save energy we switch the sensor on and off by toggling the power supply to the FDC. At first the FDC wouldn't communicate on the I2C line but when we added a 5ms delay it worked. We also tried 2ms but it didn't work.
So questions:
1) How long time does the FDC1004 need to start up and begin measuring (disregarding any capacitance on the VDD)? I'm not sure if the issue is in the MCU or in the FDC.
2) When we start-up the FDC1004 we can see a peak current of 3.9mA. Is that normal? We expected 750uA at most.
Our design is copy pasted from the evaluation board except for different MCU and sensing part.
Best regards
Johannes