This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP117: TMP117 temperature error issue

Part Number: TMP117

Hi ,all

      I have two TMP117 (QFN Footprint) , I2C communication are OK , but  they show the temperature value is more different even though int the same environment , one of them value is 26.1 ℃ ,another one value is 26.6 ℃ , what is the trouble of them ?