This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
You can familiarize yourself with how FMCW mmWave sensors operate with the following resources: http://www.ti.com/lit/spyy005
Two active mmWave sensors could theoretically cause interfence with each other. Please refer to these resources to see how interference between sensors manifests: https://training.ti.com/mmwave-awr1x-interference-detection-crucial-step-effective-mitigation?context=1128486-1139154-1135822
https://training.ti.com/managing-interference-fmcw-radar-systems
https://www.ti.com/lit/pdf/swra662
It seems you are proposing to intentionally create interference?
Amanda
I am proposing to measure the distance between two devices!
Please refer to the example link I provided. In this implementation, wideband pulsed radar is utilized but in theory similar implementation can be achieved with wideband FMCW radar (or at least we think so). In the example, the transmitter sends a narrow pulse and starts a timer at the same instant, after x amount of time the signal is received at the receiver which gets retransmitted after a fixed and known amount of time. After another x period, the transmitter receives the retransmitted signal and has enough information to extract the distance btw the two devices. This is obviously over simplified but is the basis for this example. Modulation techniques might need to be implemented in a multi-sensor environment but that also can be done. Is there anything in the hardware that prevent us from doing something like this? Thanks!
Hello,
As in my previous post it seems referring to the interference resources would be relevant to your objective as the illustrate how one radar sensor can (typically unintentionally) receive transmission from another sensor. Of course in your case you would want to do the opposite of the interference mitigation techniques.
In your scheme it should be possible to use have mmWave sensor configured with a zero slope chirp so the receivers are on but no transmission while another sensor is chirping. You can refer to the the TRM and DFP documentation for limitations that could affect this scheme: https://www.ti.com/lit/pdf/swru522 and http://downloads.ti.com/ra-processors/esd/MMWAVE-DFP/latest/exports/mmWave-Radar-Interface-Control.pdf
Amanda
Very interesting use of the radar. So, it is possible then it would seem to use two IWR6843 to measure distance between them by placing one end as transmitter and the other end as receiver?
If distance were the only objective , wouldn't an IMU sensor give you similar data? i.e., knowing GPS co-ordinates one could calculate heading and distance when a magnetometer, accelerometer, gyroscope combo sensor at both ends?
I'm interested in the same idea , but different application. Using IWR6843 as aiming tool besides sensing ,Assuming that there is an out of band control plane to reach both ends of the link.
Venkat