Hi,
We want to implement a collision warning function on a 6-axis collaborative robot, which can be automatic stop when approaching people.
We want to build some capacitive sensors on FPC and attach it to the surface of the robotic arm. The question is, since the arm is made of metal, the sensor can detect it, how to shield the metal influence?
Maybe some insulation are needed but we don't want it too thick for appearance concern.