The data sheet states the following for the TDV7201
Section 1 Features
Measurement Range:
– Individual Mode 1: 12 ns to 2000 ns
– Individual Mode 2: 250 ns to 8 ms
– Combined Operation: 0.25 ns to 8 ms
and in Section 8.1 Application information
... wide measurement range of 0.25 ns to 8 ms
I am most interested in the combined operation so that I can measure targets between near zero and 50 uS with a LIDAR system. I can see the application note for using the combined operation to get a minimum measurement, but there is no mention of how to achieve a maximum measurement in this mode. Combination mode seems to bridge the measurement range of mode 1 that is < 2uS and mode 2 that is > 250 nS, in a single measurement. Can you please clarify?
Regards