This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Usage of ready build firmware from lab's ES1

Part Number: IWR6843AOP
Other Parts Discussed in Thread: IWR6843

We try to use ready build firmwares from the lab19 in our proof of concept design. Our system consist IWR6843 antenna board, boost platform and raspberry pi4. Our IWR6843 version is ES1 (as said this is PoC) but we have already ordered ES2 antenna board also.

Problems what we phase are mostly robustness of the system. For example we need to reset boost platform between configuration changes, otherwise system starts to respond weirdly. Also when we use same configuration than in lab, the respond for 'AccelerationParam' is that it is not supported CLI command. We don't get that when running demo in the pc. We use lab19 binary from industrial_toolbox_3_6_2.

Are ready made binaries robust enough to be used in demos/PoC's? Do you think that changing some configurations might help us to achieve our target?

Br,

Sami Nummelin