Hello,
In a cascade configuration, would there ever be a situation where the SOP signals for different AWR chips would not be the same, or can these signals be tied together?
Thanks,
Robert
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
In a cascade configuration, would there ever be a situation where the SOP signals for different AWR chips would not be the same, or can these signals be tied together?
Thanks,
Robert
Hello Robert,
If you are always loading the firmware over SPI interface and not using the serial flash to store the firmware then you can use came SOP controls for all chips. Please note that SOP pins should not be driven strongly on the board or from host, they must be driven via a series 10k ohms resister since after bootup these pins became output from the AWR device.
regards,
Vivek
Additionaly , its recommended to have separate nReset controls for multiple AWr chips.
Regards,
Vivek