Tool/software: Code Composer Studio
Hi,
I am working on LDC1614 with delfino79D to measure the gap between a coil and metalic surface, i made a function that depends on 20 inductance samples measured at [0 to 19 mm] gap and used this function to measure the accurate gap using linear interpolation method.
When using the internal coils from the sensor PCB which have the same Capacitance, inductance, and resistance, i found that the error in the coil connected to CH0 is differ from the one connected to CH1.
Note that all configurations are the same for both two coils and also i measured the inductance and capacitance and also was identical for both LC sensors.
Finally i checked on all calculations in the code and it was also identical, the i have two questions here.
1- what is my problem here with the coil connected to CH0 !
2- in section ''7.3.4 Reference Clock'' in data sheet what does he mean by [ Each channel has a dedicated divider configuration.], is this when using different coils with different specifications or he mean what !!