specifically, can I use this library on nvidia xavier processors?
Thanks.
Dan.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
specifically, can I use this library on nvidia xavier processors?
Thanks.
Dan.
Hi Dan,
The MMWAVE-SDK itself is available for Windows and Linux, which means you can install the SDK to develop mmWave applications for TI devices on either Windows or Linux, however in both cases the mmwave application source code is cross-compiled to generate a binary for the selected target TI mmWave device.
If your question is whether you can run the SDK Linux installer on the NVIDIA Xavier processor (I'm assuming there will be some version of Linux running on it), i.e. to develop mmWave application using the Xavier itself as a development platform, then it is not supported.
Regards
-Nitin
Are the libraries that parse the targets able to be compiled on the Xavier or are the libraries closed source for x64 only?
If closed source, is my only option for reading the targets to write a customer parser for the data coming over the serial line? (1843 with control serial and data serial)
Thanks
Dan
Hi Dan,
We provide source code for all the visualizers (i.e. output parsers which also send the configurations commands to the corresponding demo running on the device).
Please refer to the following thread for a related discussion:
CCS/IWR6843ISK: IWR6843 ISK - Sensor Start & Stop in linux
Regards
-Nitin