The storage of the integrated DDR of tsw1400 is 1GB, but when my parameters are set to frame period 20ms, frame number 500, pulse number within a single frame 128, single pulse sampling point 175, single pulse period 70us, I calculated 500 * 128 * 175 * 16 (data is stored in 16bit) / 8 = 224000000 bytes, about 21MB, this value is far less than 1GB, but my experiment proves that such a setting cannot be successfully counted, when I change the number of frames It is 200, and the other parameters remain unchanged. At this time, data can be collected smoothly. What is going on?