Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Dear sir:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Dear sir:
Currently using the internal SBL example of "mmwave_sdk_03_03_00_03",
the makefile can be used normally, but I want to build a project to use CCS,
and use xdc110 to debug and modify the function. If there are any problems,
the error message will appear in the established project.
Provide an established good project (.projectspec), thank you.
Hi,
You should be able to load the binary xwr68xx_sbl_mss.xer4f generated by makefile in CCS and debug.
Thanks
Yogesh
Dear sir:
If I create new sbl project in CCS, currently experiencing setup issues as follows:
(1)The makefile question:
"Properties->Build->Makefile genreation->Generate Make files automatically"
Does this option need to be selected? or use the "C:\ti\mmwave_sdk_03_03_00_03\packages\ti\utils\sbl\makefile"
(2)Linker command file question:
"Properties->General->Project->Linker command file"
setting sbl_linker.cmd or others?
Thank you!
G.H lin
Before I try and help you with the CCS project, I will like to understand your concerns using gnu makefile from command-line.
Since even if you make the SBL compile using CCS project using the makefile from SDK, you will not be able to use other CCS features like changing the compiler options, adding new CFLAGS etc.
Thanks
Yogesh
Hi Yogesh :
I am currently using CCS to build an SBL project, which can be compiled successfully and produce "xwr68xx_sbl_demo.bin". After burning with the uniflash tool, the program cannot enter the main program of SBL to execute without directly executing the main program of Meta Image 4. What needs special attention in the setting of CCS.
Thanks
G.H lin
Hi G.H lin,
To verify if you have right setup, could you please tell if you are able to run pre-built binary xwr68xx_sbl.bin.
Thanks
Yogesh
Hi Yogesh:
This is my message to implement the compiler:
rm -f C:/Users/mmWave/workspace_v9/bootloader10/bootloader10.bin
makefile:194: recipe for target 'pre-build' failed
process_begin: CreateProcess(NULL, rm -f C:/Users/mmWave/workspace_v9/bootloader10/bootloader10.bin, ...) failed.
make (e=2): The system cannot find the file specified系統找不到指定的檔案。
gmake[1]: [pre-build] Error 2 (ignored)
My pre-build steps are set as follows:
rm -f ${PROJECT_ROOT}/${ProjName}.bin
Operating system uses win10
Thanks
G.H lin
Hi,
Sorry, I wanted to know if you are able to run the SBL binary in SDK 3.3:
C:\ti\mmwave_sdk_03_03_00_03\packages\ti\utils\sbl\xwr68xx_sbl.bin
The procedure is documented in:
C:\ti\mmwave_sdk_03_03_00_03\packages\ti\utils\sbl\docs\SBL_design.pdf
Thanks
Yogesh