Other Parts Discussed in Thread: TDC1000, TDC7200, TUSS4470
Hi Team,
There is a big customer use TDC1000-Q1.
Several signal was used to trigger ultrasonic device. Customer use several sine wave signal to calculate the time.
The Echo Qualification Threshold level was set to -50 mV. They find that the delay time between LNAOUT and STOP are different. Sometime the second sine wave trigger the Stop, sometime the third sine wave trigger the Stop. See the picture below.
Customer copied the schematic of TDC1000EVM. They also tried on the EVM of TDC1000. It has the same problem. Could you check it for us? I appreciate it if you can help.
Second Sine Wave trigger the STOP:
The Third Sine Wave Trigger the Stop:
BR
Songzhen Guo