Hi Experts,
I'm using LDC1101EVM for detecting metal thickness. Basically I'm reading the strength of the inductive response to do so. So, I have two seperate metal peices made of Aluminium. When I place one metal in front of the sensor it shows some values as it depends on how far I place, similiar thing I'm doing with second metal peice. But, when I'm combining the two metal peices as one it shows the same value as like single layer metal peice. I'm reading the inductance count. How is this possible? I have configured following registers:
1) RP_SET as 0x36
2) TC1 as 0xDE
3) TC2 as FE
4) DIG_CONFIG as 0xEF
5) START_CONFIG as 0x00
Can you say why I'm getting same value in both the cases (in single layer and as well as in double layer) ? I shall be grateful for that.
EDIT 1 : Does the inductance value will change according to temperature??