Hello Support team.
Firmware is mmWave DFP.
Configuration data is the data set via SPI using API of Firmware(mmWeve DFP).
This configuration data has Charp setting, Frame structre , CSI setting and so on.
From APN “AWR1243 Bootloader Flow” , Firmware can be stored in serial Flash Memory connected with AWR1243P.
But I would like to know if the above configuration data can be stored in serial Flash Memory connected with AWR1243P.
if yes, I would like to know how to stored it and what format data need to be converted.
Best Regards
KORO