Other Parts Discussed in Thread: TMP116,
Similar to the previous post titled "TMP116: Polling the data ready flag seems to clear it inadvertently", I too am not getting a Data Ready for each 1-shot request I submit.
If I set the TMP117 up to perform 1-shot requests once per second, about 16% of the time, the Data Ready bit does not get set and I time out (regardless of if the timeout is 200 ms or 5 seconds!).
If I set the TMP117 to Continuous Capture mode and poll the Data Ready bit every second, I get no timeouts whatsoever.
It's as if either (a) the 1-shot request is not seen or (b) the Data Ready bit is somehow cleared without me seeing it.
I am doing no other operations to the device.
Has anyone else seen a similar behavior from the TMP117?