Other Parts Discussed in Thread: TDC1000, TDC1011
Hello,
I am testing the module TDC1000-C2000EVM using a transducer of 2.4MHz, and I tried to follow the steps in this document 
I connect just one transducer as transmitter and receiver, and I do not receive any eco signal. Is correct connect TX1 and RX2 in mode 0 or TX1 and RX1 in mode 1, to have connected just one transducer?
I connected the transducer to TX1 and GND on Mode 0 into the J5 connector.
I saw this document, and I need to do application N#1 Fluid Level (see page 5)

In that document on Figure 5, it is connected TX and RX, my question is that if I have to connect TX1 and RX2 to the same terminal of the transducer and the other to GND on mode 0 ?
Also which is the recommended configuration for this application on the GUI?
Regards
Heiner