Other Parts Discussed in Thread: DCA1000EVM, AWR2243
Dear TI-Support,
I am taking AWR2243 Boost + DCA1000EVM in operation. I have succeded in downloading the BSS and MSS FW. After this step I also succeed with SPI connect.
When I turn RF Power-Up there is no response, in the log output following message appears:
--------------
[23:11:23] [RadarAPI]: Status: Passed
[23:11:29] Device Status : UnDetDe/ASIL-B/SOP:2/ES:0
[23:11:29] [RadarAPI]: ar1.RfEnable()
[23:11:34] Status: Failed, Error Type: RESP TIMEOUT
[23:11:38] BSS Power Up async event was not received!
--------------
BSS FW: C:\\ti\\mmwave_dfp_02_01_05_03\\firmware\\radarss\\xwr2xxx_radarss_rprc.bin
MSS Fw C:\\ti\\mmwave_dfp_02_01_05_03\\firmware\\masterss\\xwr22xx_masterss_rprc.bin
Please help.
Regards
Prasanna