Greetings,
I have recently being testing with the IWR6843AOPEVM for obstacle avoidance in a mobile robot. The sensor is mounted on top of the robot (2m up) in standalone version and although it works well in general, there seems to be an frequent detection of "ghost" points (the points appear at varied distances and angles). I read that the bouncing of the signal in corners can cause such false positives but the test area is quite open, 6m x 6m and I imagine this could minimize the issue. I have tried decreasing the sensor sensitivity but that affects the obstacle detection capabilities. Furthermore, I have also implemented some KNN algorithms to detect noise but due to the sparse cloud that also affects the obstacle detection capabilities.
Do you know what could be the cause of the false positives? Is such a behavior expected? What would you recommend doing in such a scenario?
Thanks in advance.
Kind regards,
Felipe Xavier