This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

awr1243+DCA1000 Frame config

Other Parts Discussed in Thread: AWR1243

Hello everyone!
I use awr1243 + DCA1000 to collect data, and I have questions when setting Frame. I know Frame time = (Ramp end time + Chirp Idle time) * Total number of chirps, but when I set Ramp end time to 50us, Chirp Idle time to 10us, 200 frames in mmwave studio, theoretically Frame Periodicity should be ( 50 + 10) * 200 = 12ms, but when I set it to 12ms, it reported an error, the error was "Frame On Time <Frame Periodicity", I understand the literal meaning of this error, but I do not understand why this is the case. I want to make the frames seamlessly connected, but according to the above, it can't be achieved. What is going on?
Han