This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWAVE-STUDIO: how to measure the TX power of IWR6843 at single frequency?

Part Number: MMWAVE-STUDIO
Other Parts Discussed in Thread: IWR6843

for the RF performance test including an antenna performance

i would like to measure the TX power from the IWR6843 Radar board at single frequency

for example measuring the output power at 60GHz, 61GHz, 62Ghz, 63GHz, 64Ghz.

then do i have to use "ConStream"?

look forward your answer

thank you