According to our customer's request, I would like to make a firmware without RTOS on IWR6843.
Until now, I have only developed RTOS-based firmware using mmwave SDK,
Is it possible to operate the firmware without RTOS?
Best Regards,
Hiroyuki Taguchi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
According to our customer's request, I would like to make a firmware without RTOS on IWR6843.
Until now, I have only developed RTOS-based firmware using mmwave SDK,
Is it possible to operate the firmware without RTOS?
Best Regards,
Hiroyuki Taguchi
Hello Hiroyuki Taguchi,
Yes you can run mmwave w/o RTOS. Please refer to following lab:
http://dev.ti.com/tirex/explore/node?node=AEIYcK.ZhaTomhvTFvAEIg__AocYeEd__LATEST
It is on older SDK and different device, but you should be able to port the same.
Thanks
Yogesh
Hi Yogesh,
Thank you for your reply.
I will check the contents of the lab in the toolbox for which I received the information.
Regards,
Hiroyuki